AXIS#.HOME.DEC
Description
This parameter sets the deceleration used while homing.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
Rotary: RPM See Acceleration Units for details. |
|
Range |
Depends on units. See Acceleration Range for details. |
|
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HOME.DEC | 0x5008 | 0x7 | UDINT | - | Acceleration | RW | False |
| AXIS2.HOME.DEC | 0x5108 | 0x7 | UDINT | - | Acceleration | RW | False |
Related Topics
Homing